AXIS#.SAFEPARAM.SBT.FUNCTIONACTIVATION
Description
Indicates whether Safe Brake Test (SBT) can be activated. When ready for activation and SBT has not been run within the specified interval, a warning is activated indicating the need to run SBT. When the SBT is set to never be active, it is not possible to execute the safe brake test and no warning is activated for SBT.
Value |
Description |
---|---|
0 |
Never active |
1 |
Ready for activation |
Context
For complete SBT information refer to SBT (Safe Brake Test).
Related safety parameters:
- AXIS#.SAFE.SBT.ERROR
- AXIS#.SAFE.SBT.MOVE
- AXIS#.SAFE.SBT.STATE
- AXIS#.SAFEPARAM.SBT.MAXAPPLOAD
- AXIS#.SAFEPARAM.SBT.MAXMOTIONBRAKE#
- AXIS#.SAFEPARAM.SBT.MAXTIMEINTERVAL
- AXIS#.SAFEPARAM.SBT.TORQUEDURATION
- BRAKE#.SAFE.SBT.ELAPSED
- BRAKE#.SAFE.SBT.STATE
Versions
Action |
Version |
Notes |
---|---|---|
Implemented |
2-00-00-000 |
Implemented in SMM revision v0.54 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0, 1 |
Default Value |
0 (Never active) |
Data Type |
Integer |
Stored in Non-Volatile Memory |
No |
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.SAFEPARAM.SBT.FUNCTIONACTIVATION |
3157h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS2.SAFEPARAM.SBT.FUNCTIONACTIVATION |
3257h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |